How to Choose the Right Robotic Joint Motor? A Complete Guide to Torque, Speed, and Integration
With the rapid development of artificial intelligence, robotic control technologies, and intelligent manufacturing, robots are evolving from traditional industrial automation equipment toward more intelligent, flexible, and autonomous systems. In recent years, emerging applications such as humanoid robots, quadruped robots, collaborative robots, and high-precision industrial robotic arms have continued to grow, creating higher requirements for core drive systems.
As a key power component of robotic motion systems, robotic joint motors directly determine a robot’s movement capability, load capacity, control accuracy, and overall reliability. Complex robotic movements such as walking, grasping, balancing, and rotation all rely on joint drive systems to provide stable and precise power output.
Unlike traditional motor applications, modern robots need to perform more complex dynamic movements. Therefore, robotic joint motors must not only provide sufficient power but also achieve fast response, high-precision control, lightweight design, and high reliability.
A high-performance robotic joint drive system typically needs to provide:
- High output torque: Meeting the requirements of robot loads and dynamic movements;
- Fast response capability: Enabling flexible and precise motion control;
- High-precision feedback: Ensuring accurate position, speed, and torque control;
- Lightweight design: Reducing overall robot weight and improving energy efficiency;
- High integration: Simplifying system structure and improving reliability.
Especially in humanoid robots, joint motors must balance power, speed, and weight. For example, leg joints need to support the robot’s own weight and withstand impact forces during movement, requiring high peak torque and excellent reliability. Robotic arm joints focus more on control accuracy, smooth motion, and repeatability.
Currently, robotic drive technology is developing toward higher torque density, compact design, and higher integration. More and more robots are adopting Integrated Robotic Actuators, which combine motors, reducers, encoders, and drive controllers into a compact unit to improve overall system performance.
Therefore, selecting the right robotic joint motor requires comprehensive consideration of output torque, speed, reduction ratio, control method, size, weight, and system integration capability to achieve efficient and reliable robotic motion.
What Is a Robotic Joint Motor?
A Robotic Joint Motor, also known as a Robotic Joint Actuator, is a core power module used to drive robotic joints. It converts electrical energy into mechanical motion, enabling robots to perform movements such as rotation, swinging, and positioning.
Unlike conventional motors, robotic joint motors must meet requirements including high torque, fast response, high precision, and lightweight design. Therefore, they usually adopt an integrated structure that combines multiple functional modules.
A complete robotic joint actuator typically includes:
- BLDC Motor: Provides power output;
- Gearbox: Increases output torque and reduces speed;
- Encoder: Provides accurate position feedback;
- Motor Driver: Controls motor operation.
Through the cooperation of these components, robotic joint motors achieve precise, stable, and efficient motion control. They are widely used in:
- Humanoid robots;
- Quadruped robots;
- Industrial robotic arms;
- Collaborative robots;
- Exoskeleton robots.
With the continuous development of robotics, joint actuators featuring high torque density, compact size, and high integration are becoming an important component of future robotic motion systems.
Core Components of Robotic Joint Motors
A robotic joint motor is not just a single motor but a highly integrated drive system, mainly consisting of:
- Brushless DC Motor (BLDC Motor)
- Gearbox
- Encoder
- Motor Driver
- Control Interface
1. BLDC Motor
The BLDC motor is the power source of the joint actuator. It features:
- High efficiency;
- High speed;
- Excellent dynamic response;
- Long service life.
Compared with traditional brushed motors, BLDC motors are more suitable for long-term and high-frequency robotic operations.
2. Gearbox
A motor usually operates at high speed, while robotic joints require higher output force. Therefore, a gearbox is used to convert speed into torque.
The main functions of a gearbox include:
- Increasing output torque;
- Reducing output speed;
- Improving load capacity.
Common reduction solutions include:
- Planetary gearbox;
- Harmonic drive;
- Cycloidal reducer.
Different reduction mechanisms affect the joint’s stiffness, accuracy, efficiency, and response speed.
3. Encoder
The encoder detects motor position and speed, making it a critical component for precise robotic motion control.
High-precision encoders enable:
- Accurate position control;
- Stable speed regulation;
- Torque control;
- Dynamic posture adjustment.
Torque: The Most Important Parameter of Robotic Joint Motors
What Is Joint Motor Torque?
Torque determines how much rotational force a robotic joint can generate.
Simply:
- Higher torque means stronger load capacity;
- Higher continuous torque means better long-term operation capability;
- Higher peak torque means stronger instantaneous movement capability.
For humanoid robots:
- Hip and leg joints must support body weight and withstand motion impacts, requiring high peak torque;
- Arm and wrist joints focus more on weight, precision, and torque density.
When selecting a robotic joint motor, factors such as:
- Robot weight;
- Payload;
- Joint position;
- Dynamic motion requirements;
must all be considered.
For example, a robotic arm carrying a 5kg object and a humanoid robot supporting its own body weight have completely different torque requirements.
Speed: Affecting Robot Motion Speed and Response Capability
Besides torque, speed is another important factor when selecting robotic joint motors.
If motor speed is too low:
- Robot movement becomes slower;
- Dynamic response decreases.
If motor speed is too high:
- Control becomes more difficult;
- Requirements for the reduction system increase.
Therefore, robotic joint design is not about pursuing the highest speed, but finding the best balance between speed, torque, and control stability.
Different robots have different speed requirements:
Humanoid Robots
Focus on:
- Fast leg movement;
- Dynamic balance;
- High-response control.
Quadruped Robots
Focus on:
- Explosive power;
- Fast jumping;
- Impact resistance.
Industrial Robotic Arms
Focus more on:
- Accuracy;
- Stable operation;
- Repeat positioning capability.
How Does Reduction Ratio Affect Robotic Joint Performance?
Reduction ratio is a key parameter affecting robotic joint performance. It determines:
- Output torque;
- Output speed;
- Control response.
Low Reduction Ratio
Advantages:
- Faster response;
- Better backdrivability;
- More flexible movement.
Suitable for:
- Humanoid robots;
- Exoskeleton robots.
High Reduction Ratio
Advantages:
- Higher output torque;
- Stronger load capability.
Suitable for:
- Industrial robots;
- Heavy-duty robotic arms.
Therefore, robotic joint design requires balancing torque, speed, stiffness, and flexibility.
Integrated Design: Why Are More Robots Using Integrated Actuators?
Traditional robotic joints usually use:
Motor + Gearbox + Encoder + Driver
as separate components.
This approach has disadvantages:
- Complex structure;
- More wiring;
- Larger installation space;
- Higher debugging costs.
Integrated robotic joint actuators combine multiple modules into one compact unit, providing:
More Compact Design
Reducing external connections and improving space utilization.
Easier Installation
Reducing development and debugging complexity.
Higher Reliability
Fewer connection points improve long-term stability.
Better Suitability for Intelligent Robots
Supporting:
- CAN;
- CAN FD;
- EtherCAT;
- RS485.
This allows multiple joints to work together efficiently.
How to Choose Joint Motors for Different Robot Applications?
| Application | Key Requirements | Recommended Features |
|---|---|---|
| Humanoid Robots | Torque density, response speed | Lightweight, high peak torque, high integration |
| Quadruped Robots | Explosive power, reliability | High torque, high stiffness, impact resistance |
| Collaborative Robots | Precision, safety | Low noise, high control accuracy |
| Industrial Robots | Load capacity, stability | High reliability, long lifetime |
| Exoskeleton Robots | Weight, efficiency | Compact size, high efficiency |
Key Parameters When Selecting Robotic Joint Motors
1. Output Torque
Pay attention to:
- Continuous torque;
- Peak torque;
- Maximum load.
2. Speed Range
Select the appropriate speed based on:
- Robot motion requirements;
- Control requirements.
3. Size and Weight
For mobile robots:
Weight directly affects battery life, motion efficiency, and overall robot performance.
4. Encoder Accuracy
High-precision encoders provide:
- More accurate position feedback;
- More stable motion control;
- Better torque control.
5. Communication Methods
Modern robots usually require support for:
- CAN;
- CAN FD;
- EtherCAT;
- RS485.
This enables coordinated control between multiple joints.
Future Development Trends of Robotic Joint Motors
Future robotic drive systems will develop toward:
Higher Torque Density
Meeting the lightweight requirements of humanoid robots.
Higher Integration
Further integration of motors, drivers, and sensors.
Smarter Control
Combining:
- AI algorithms;
- Force control technology;
- Real-time feedback;
to achieve more natural human-robot interaction.
Higher Reliability
Through:
- Potting technology;
- Thermal management design;
- Advanced materials;
to improve long-term robotic operation capability.
Conclusion
Selecting the right robotic joint motor requires comprehensive consideration of torque, speed, reduction ratio, control accuracy, and system integration capability. Different robotic applications have different performance requirements. For example, humanoid robots focus more on high torque density, fast response, and lightweight design, while industrial robotic arms emphasize stability, precision, and long-term reliability.
Torque determines robotic strength, speed affects motion performance, reduction ratio balances overall capability, and integration improves system efficiency and reliability. Only by properly matching these key parameters can more precise and efficient robotic motion control be achieved.
As robots continue to become more intelligent and lightweight, integrated robotic joint actuators will become an essential trend for future robotic systems. By combining motors, gearboxes, encoders, and drive systems, they can reduce structural complexity while improving overall robotic performance.
In the future, robotic joint motors will continue to evolve toward higher torque density, smaller size, higher precision, and smarter control, providing more reliable power solutions for humanoid robots, quadruped robots, and next-generation intelligent robotic systems.