Frameless Outer Rotor Motor vs Inner Rotor Motor: How to Choose for Robotics Applications?

Frameless Outer Rotor Motor vs Inner Rotor Motor: How to Choose for Robotics Applications?

In today's rapidly evolving robotics landscape, the motor is no longer just a basic component that "provides rotational power"—it has become a core actuation unit that directly determines the upper performance limits of the entire system. Especially in humanoid robots, quadruped robots, and high-precision collaborative robotic arms, the motor's structural form profoundly affects the system's force control capability, dynamic response, spatial layout, and long-term reliability.

From an engineering design perspective, motor selection has long since progressed from "whether it can spin" to a system-level question of "how stable it spins, how precisely it is controlled, and how compactly it integrates." Against this backdrop, frameless outer rotor motors and inner rotor motors have emerged as the two most frequently compared technological paths.

The two may appear to differ only in "rotor position," but they essentially represent two entirely distinct design philosophies:

  • One emphasizes high torque density and structural integration (oriented toward robotic joints)
  • The other emphasizes mature reliability and high-speed versatility (oriented toward traditional industrial drives)

Understanding their structural differences is the first step in robotic joint design, electric drive system selection, and overall system architecture optimization.

Below, we start from the basic structure and break down the core distinctions between these two motor types.

Definitions: Frameless Outer Rotor Motor vs Inner Rotor Motor

What is a Frameless Outer Rotor Motor

A frameless outer rotor motor is a core motor component that omits the housing, bearings, and encoder—typically retaining only the stator and outer rotor—and is designed to be directly integrated by the user into the robotic or mechanical structure.

It is not a "complete motor" in itself, but rather an embedded power module, specifically designed for high-integration equipment, particularly robotic joints.

1.Structural Characteristics

A typical frameless outer rotor motor features:

  • Stator fixed on the inside
  • Rotor located on the outside and rotating around the stator
  • No motor housing
  • No bearing system
  • No pre-installed encoder (typically integrated at the system level)

Think of it as:

"Taking apart" a conventional motor and keeping only the electromagnetic core.

2.Why is it called "Outer Rotor"?

"Outer rotor" means:

  • The rotor rotates on the outer circumference
  • The load is typically connected directly to the outer rotor
  • Larger moment arm → naturally enables higher torque output

This structure is particularly suited for:

  • Low-speed, high-torque applications
  • Direct-drive joints
  • Space-constrained designs

What is an Inner Rotor Motor

An inner rotor motor is the most common motor structure, characterized by the rotor located inside the motor and the stator on the outside, with mechanical power output delivered through an output shaft driven by the internal rotating rotor.

Simply put:

"The shaft spins in the middle, while the housing remains fixed"—the conventional motor structure.

1.Basic Components

An inner rotor motor typically consists of:

  • Rotor: located at the center, responsible for rotational output
  • Stator: located on the outside, generating the electromagnetic field
  • Motor housing: provides support and heat dissipation
  • Bearing system: supports high-speed rotation
  • Output shaft: transmits torque

2.Working Principle

The inner rotor motor operates as follows:

  1. The stator is energized to generate a rotating magnetic field
  2. The rotor is "dragged" into rotation by the magnetic field
  3. The rotor drives the central output shaft to deliver torque
  4. Mechanical energy is converted into power output

 

Impact of Core Structural Differences on Performance

Comparison Dimension Frameless Outer Rotor Motor Inner Rotor Motor

Torque Output Higher (outer rotor leverage) Medium to high

Speed Capability Better at low-to-medium speeds Stronger high-speed performance

Heat Dissipation Excellent (more open structure) Dependent on housing design

Integration Method Highly integrated (requires Plug-and-play
structural design)

Control Precision High (suitable for force Medium
control)

Cost Higher Relatively lower

 

Why Are Robots More Biased Toward Frameless Outer Rotor Motors?

In modern robotic system design—particularly humanoid robots, quadruped robots, and high-DOF manipulators—the adoption rate of frameless outer rotor motors is rising rapidly. This trend is not driven by a single technical preference, but by the combined demands of robotics for torque density, structural integration, and dynamic control capability.

From a systems engineering perspective, the motor in a robot is no longer merely a "power output component," but a core element directly participating in joint control, motion precision, and overall structural design. Therefore, under identical volume and weight constraints, achieving higher output capability and superior control performance becomes the key selection criterion.

1.Higher Torque Density for Compact Joint Design

Due to the externally located rotor with its larger moment arm, frameless outer rotor motors deliver higher torque within the same volume. This is particularly critical for space-limited robotic joints (e.g., knees, hips, elbows), enabling significant drive force increases without enlarging the joint footprint.

2.Better Suited for Direct-Drive or Low-Reduction Architectures

Modern robots increasingly reduce reliance on complex reduction systems, opting for direct-drive or low-reduction designs for higher efficiency and lower backlash. Frameless outer rotor motors excel in low-speed, high-torque output, making them easier to implement for high-precision force control and smooth motion.

3.Higher System Integration and Structural Freedom

The frameless design means the motor is no longer a standalone finished product, but can be directly embedded into the mechanical structure, enabling integrated design with joint housings, bearing systems, and even reduction mechanisms. This significantly reduces wasted volume, making robot joints more compact and efficient.

4.Superior Dynamic Response and Control Consistency

With more favorable inertia distribution, frameless outer rotor motors deliver more stable torque output under low-speed, high-load conditions, making them better suited for complex dynamic actions (e.g., running, jumping, grasping). They also facilitate higher-bandwidth control, improving overall motion precision.

 

Advantages of Inner Rotor Motors in Specific Scenarios

Although frameless outer rotor motors are gradually becoming the mainstream choice in robotic joints, inner rotor motors—with their mature structural systems and broad industrial adaptability—remain irreplaceable in many applications. Their core value lies in high-speed performance, cost efficiency, and standardization, making them highly suitable for traditional industrial and general-purpose drive systems.

1.High-Speed Rotation Applications

Inner rotor motors, with their centrally located rotor and lower rotational inertia, perform more stably at high speeds, enabling higher rotational speeds and superior dynamic response.

Typical applications include:

  • Fan systems
  • Pumps and fluid drive equipment
  • Industrial spindles and high-speed tools

Advantages: high-speed efficiency, smooth operation, mature vibration control

2.Cost-Sensitive Industrial Equipment

In large-scale industrial applications, cost control and supply chain stability often outweigh extreme performance. Inner rotor motors benefit from high standardization and mature manufacturing processes, offering clear cost advantages.

Suitable for:

  • Automated production line equipment
  • Standard industrial drive systems
  • General-purpose motor replacement solutions

Advantages: low cost, easy procurement, easy maintenance

3.Mature Reduction System Integration

Inner rotor motors have a well-established compatibility with various reduction mechanisms (e.g., planetary gears, synchronous belt systems) and are widely used in conventional servo drive architectures.

Suitable for:

  • Industrial robotic arms (traditional architectures)
  • Logistics conveyor systems
  • Automated assembly equipment

Advantages: strong system compatibility, low engineering risk

4.Scenarios with Low Structural Integration Requirements

When extreme compactness or joint-integrated design is not required, the "plug-and-use" advantage of inner rotor motors becomes more apparent.

Suitable for:

  • Standard equipment retrofits
  • Modular industrial equipment
  • Non-joint-type drive systems

Advantages: simple design, low integration cost

 

Core Metrics for Robotics Motor Selection

In robotic motor selection, structural form (frameless outer rotor vs. inner rotor) is only the first step. The more critical task is to comprehensively evaluate motor performance across power capability, control precision, thermal management, and mechanical adaptability based on system requirements. Different application scenarios place varying emphasis on these metrics, ultimately determining whether a motor truly fits the overall system.

1.Torque Performance (Rated Torque / Peak Torque)

Torque is the most fundamental output metric for robotic motors, directly determining joint load capacity and motion performance.

  • Rated torque: determines long-term continuous operation capability
  • Peak torque: determines instantaneous burst capability (e.g., jumping, grasping, impact actions)

In humanoid and quadruped robots, peak torque is particularly critical.

2.Torque Density (Nm/kg)

Torque density is a core metric measuring "performance per unit volume/weight," directly affecting structural design freedom.

  • High torque density → smaller joint volume
  • More suitable for compact robot designs

Frameless outer rotor motors typically have an advantage here.

3.Dynamic Response Capability (Response Speed / Control Bandwidth)

Dynamic response determines whether the robot can "keep up with control commands."

This includes:

  • Acceleration capability
  • Response latency
  • Control bandwidth (FOC control effectiveness)

Especially important for high-speed motion robots (e.g., quadrupeds).

4.Inertia Matching

Proper inertia matching significantly improves control stability and energy efficiency.

  • Excessively high inertia → slow response
  • Excessively low inertia → insufficient stability

A critical yet often overlooked factor in robotic joint design.

5.Heat Dissipation and Thermal Stability

Motors generate substantial heat under sustained high-load operation; heat dissipation capability directly affects sustained performance.

  • Good thermal design → higher continuous torque output
  • Less thermal derating → more stable control

Frameless structures offer greater flexibility in system-level thermal design.

6.Control and Communication Capability

Modern robotic motors are often not just "motors" but intelligent actuation units.

Common metrics include:

  • Encoder resolution (position accuracy)
  • Control modes (velocity / position / torque)
  • Communication protocols (CAN / EtherCAT, etc.)

High-end robots favor high-bandwidth real-time control systems.

7.Structural Dimensions and Integration Compatibility

Whether the motor fits the robotic joint space is one of the most practical constraints in selection.

  • Supports joint-embedded design?
  • Supports integrated actuator architecture?
  • Installation space limitations?

Directly impacts the overall mechanical design approach.

Robotic motor selection is not a single-metric decision, but a comprehensive system optimization process. In practical engineering, a balance must be struck among torque performance, volume constraints, dynamic response, and control capability to ultimately select the motor solution best suited for the specific robotic architecture.

 

Comparison of Robotics Application Scenarios

Different robotic systems have widely varying performance requirements. The following table compares frameless outer rotor motors and inner rotor motors in typical applications:

Robotics Application Type Performance Requirements Recommended Motor Type Selection Rationale

Humanoid Robots High torque density, compact structure, Frameless outer rotor motor Limited joint space, requires high integration and direct-drive
high-precision force control, low-speed capability, ideal for high-DOF motion control
high torque

Quadruped Robots High dynamic response, shock load Frameless outer rotor motor Withstands impact from running and jumping; outer rotor
tolerance, burst capability, frequent + reducer structure better suited for high-torque dynamic output
motion changes

Collaborative Robots High safety, high precision, medium Hybrid (outer rotor / High-load joints use outer rotor, low-load axes may use
load, stable operation inner rotor) inner rotor for performance-cost balance

Industrial Automation Equipment High-speed rotation, low cost, long-term Inner rotor motor Mature standard structure, suitable for batch applications
stable operation, easy maintenance and high-speed operation

Frameless Outer Rotor Motors: More suitable for robotic joints and high-performance dynamic systems
Inner Rotor Motors: More suitable for industrial automation and high-speed standardized applications
Hybrid Architectures: The current mainstream trend in complex robotic systems

 

Conclusion

Against the backdrop of rapid robotics evolution toward high-DOF, intelligent, and lightweight designs, the motor has transitioned from a conventional "power source" to a core actuation unit that affects overall system performance. The choice between frameless outer rotor and inner rotor motors fundamentally reflects two distinct engineering pathways: one oriented toward highly integrated, high-torque-density robotic joint systems, and the other toward mature, stable, high-speed general-purpose industrial drives.

Structurally, inner rotor motors leverage "high-speed rotation + standardized output" as their core advantage, offering low cost, mature technology, and broad applicability, and have long dominated industrial automation and high-speed rotating equipment. Frameless outer rotor motors, on the other hand, emphasize "high torque density + modular integration," leveraging a larger moment arm and embedded design capability to demonstrate clear advantages in robotic joint systems.

From an application perspective, highly dynamic systems such as humanoid and quadruped robots rely more on frameless outer rotor motors to achieve high torque output and precise force control within compact structures; while industrial automation equipment and high-speed rotation scenarios continue to use inner rotor motors as stable and reliable baseline solutions. In complex systems, the two often coexist in hybrid architectures to strike a balance between performance and cost.

Overall, motor selection is no longer a matter of choosing a single component, but rather part of system-level architectural design. Looking ahead, as robots evolve toward highly integrated joints and direct-drive structures, the importance of frameless outer rotor motors will continue to grow, while inner rotor motors will maintain their irreplaceable stable position in traditional industrial domains.

From a selection logic standpoint, the core distinction between "frameless outer rotor motors" and "inner rotor motors" lies in torque density and system-level application fit—and this is the key dividing line in robotic motor design.

Back to blog