How Does Gear Ratio Affect Robot Joint Performance?

How Does Gear Ratio Affect Robot Joint Performance?

In today's rapidly developing robotics industry, joint performance has become one of the key factors determining overall robot performance. Whether it is humanoid robots, quadruped robots, or industrial manipulators, the joint's output capability, dynamic response, and control precision directly affect the overall motion performance and task execution capability.

Among the many parameters affecting joint performance, "reduction ratio" is a core metric that is frequently mentioned but easily misunderstood. It is not only related to the conversion efficiency between torque and speed, but also affects the

 system's stability, controllability, and applicable scenario range. Under different application requirements, even with the same motor and reducer combination, simply adjusting the reduction ratio can produce significant differences in overall robot performance.

Therefore, understanding the essence of reduction ratio and its impact on robot joint performance is of great significance for rational motor selection and joint design.

 

What is Reduction Ratio?

Reduction Ratio (Gear Ratio) is a key parameter describing the relationship between the input shaft speed and output shaft speed of a reducer, and is commonly used to measure the "conversion ratio between speed and torque" in mechanical transmission systems.

Simply put, reduction ratio is:

Input Speed ÷ Output Speed = Reduction Ratio

For example:

  • A reduction ratio of 10:1 means the input shaft rotates 10 times while the output shaft rotates 1 time
  • A reduction ratio of 50:1 means the input shaft rotates 50 times while the output shaft rotates only 1 time

In this process, energy is not created out of thin air, but rather the conversion relationship of speed reduction + torque amplification is achieved through gear structures (under ideal conditions, losses are not considered).

From a physical perspective, the core function of reduction ratio is to achieve "energy redistribution" in mechanical systems:

  • Converting the motor's high-speed, low-torque output
  • Into the joint's low-speed, high-torque output

Therefore, in robot joint systems, reduction ratio is not just a simple proportional parameter, but one of the key design variables determining overall system performance.

In practical engineering applications, reduction ratio typically needs to be designed by comprehensively considering the following factors:

  • Motor rated speed and torque
  • Joint load magnitude
  • Target motion speed range
  • Control precision requirements
  • System volume and weight constraints

Different reduction ratio choices will directly lead to significant differences in robot power and flexibility.

 

How Does Reduction Ratio Affect Robot Joint Performance?

1. Impact on Output Torque: Determining the "Strength Ceiling"

The most direct effect of reduction ratio is on output torque.

Under ideal conditions:

Output Torque = Motor Torque × Reduction Ratio × Transmission Efficiency

Therefore:

  • Higher reduction ratio → Higher output torque
  • Lower reduction ratio → Lower output torque

This means:

  • High reduction ratio joints are more suitable for bearing heavy loads, e.g., hip joints, knee joints
  • Low reduction ratio joints are more suitable for lightweight, high-speed motion, e.g., wrist joints or dexterous hands

Essentially, reduction ratio is a trade-off between "speed" and "strength"

2. Impact on Motion Speed: Determining "Dynamic Performance"

Reduction ratio is inversely proportional to output speed:

Output Speed = Motor Speed ÷ Reduction Ratio

Therefore:

  • Higher reduction ratio → Slower joint motion
  • Lower reduction ratio → Faster joint response

In actual robot applications:

  • Quadruped robots require rapid reactions, so they typically adopt lower reduction ratios
  • Industrial manipulators focus more on stable control, so they can use higher reduction ratios

Higher reduction ratios improve stability but reduce dynamic performance.

3. Impact on Control Precision: Determining "Motion Refinement"

Reduction ratio also significantly affects the system's control resolution.

The reason is:

  • Output-side angular change = Motor-side angle / Reduction Ratio

Therefore:

  • Higher reduction ratio → Finer output angular resolution
  • Lower reduction ratio → Lower control resolution

For example:

  • High-precision manipulators typically use higher reduction ratios to achieve finer end-effector trajectory control
  • Humanoid robots need to compromise between "precision" and "response speed"

4. Impact on Stiffness and Backdrivability: Determining "Interaction Capability"

Reduction ratio also affects the mechanical characteristics of joints:

  • Higher reduction ratio → Higher stiffness, harder to be driven by external forces
  • Lower reduction ratio → Easier to be driven by external forces (better backdrivability)

This is especially important for collaborative robots (Cobots):

  • Human-robot safe interaction required → More emphasis on backdrivability → Cannot use excessively high reduction ratios
  • Industrial fixed tasks → More emphasis on stiffness → Can use higher reduction ratios

5. Impact on Energy Consumption and Efficiency: Determining "System Burden"

Although reducers can increase torque, they also introduce certain losses:

  • Gear friction losses increase with reduction ratio and number of stages
  • High reduction ratio systems typically have slightly lower efficiency
  • Motor load distribution also changes

Therefore:

  • Excessively high reduction ratios may lead to increased system heating
  • Reasonable reduction ratios can optimize overall energy efficiency

 

Why Is Reduction Ratio Design So Important?

With the rapid development of humanoid robots, quadruped robots, and intelligent manufacturing, robot joints are evolving toward high integration, high dynamic performance, and high-precision control.

Under this trend, reduction ratio design has gradually transformed from a traditional mechanical parameter into one of the key control variables affecting overall system performance.

Reasonable reduction ratio configuration can significantly improve:

  • Motion efficiency
  • Dynamic response capability
  • Structural stability
  • Energy utilization efficiency

Conversely, unreasonable reduction ratio design may lead to:

  • Sluggish motion
  • Insufficient torque
  • Control difficulties
  • System heating and efficiency degradation

 

Reduction Ratio Selection for Different Application Scenarios

In actual robot design, there is no unified standard for reduction ratio selection; instead, it requires comprehensive trade-offs based on dynamic performance requirements, load capacity, and control strategies of different application scenarios. Different types of robots have significantly different emphases on joint performance, so reduction ratio configurations also differ markedly.

Below is an analysis based on three typical robot applications:

1.Humanoid Robots

Humanoid robots require highly comprehensive balanced systems of joint performance, needing strength, flexibility, and natural motion capability simultaneously.

Characteristics:

  • Need to simulate human motion
  • Large number of joints
  • Complex and continuous movements
  • Sensitive to weight and energy consumption

Recommended Reduction Ratio Range:

20:1 ~ 100:1

Design Focus:

  • Lower limb joints (hip, knee): Higher reduction ratio (torque priority)
  • Upper limb joints (shoulder, elbow): Medium reduction ratio (balanced type)
  • Wrist joints: Lower reduction ratio (flexibility priority)

Core Objective:

Achieve a balance among "strength + speed + degrees of freedom"

2.Quadruped Robots

Quadruped robots emphasize high-speed dynamic stability and ground adaptability, requiring fast response and high-frequency motion capability.

Characteristics:

  • High-dynamic motion (running, jumping, obstacle avoidance)
  • Frequent posture adjustments
  • Extremely high response speed requirements
  • Lightweight design priority

Recommended Reduction Ratio Range:

5:1 ~ 30:1

Design Focus:

  • Prioritize response speed
  • Control system needs high bandwidth
  • Joints need good backdrivability

Core Objective:

"Fast response + dynamic balance + lightweight"

3.Industrial Manipulators

Industrial manipulators are mainly used for high-precision, repetitive tasks, with extremely high requirements for stiffness and stability.

Characteristics:

  • High-load operations
  • High repetitive positioning accuracy requirements
  • Relatively controllable operating speeds
  • High-stiffness structure

Recommended Reduction Ratio Range:

50:1 ~ 150:1

Design Focus:

  • Maximize output torque
  • Improve positioning accuracy
  • Enhance system stiffness
  • Reduce vibration and backlash effects

Core Objective:

"High precision + high stiffness + high load capacity"

 

Application Scenario Reduction Ratio Comparison Table

Application Recommended Core Requirements Main Advantages Typical Joints
Reduction Ratio

Humanoid Robot 20:1 ~ 64:1 Balanced performance Flexibility + Hip / Shoulder / Elbow /
Stable control + Wrist
Sufficient torque

Quadruped Robot 6:1 ~ 30:1 Dynamic response High speed + Leg joints (Hip / Knee /
Lightweight + Ankle)
Fast reaction

Industrial 30:1 ~ 64:1 High precision and High stiffness + Multi-axis joints
Manipulator stable output High torque density (Shoulder / Elbow /

  • Control stability End-effector)

Different robot systems' requirements for reduction ratio essentially reflect three distinct design priorities:

  • Humanoid robots: Balanced system
  • Quadruped robots: Dynamic-priority system
  • Industrial manipulators: Precision-priority system

Therefore, in practical engineering design, reduction ratio selection must be aligned with the application scenario, rather than simply pursuing "large or small".

 

Reduction Ratio Is the Core Trade-off Parameter in Robot Joint Design

Reduction ratio not only determines the relationship between output torque and motion speed of robot joints, but also further affects the system's control precision, dynamic response capability, structural stiffness, and overall energy efficiency performance.

In different application scenarios, reduction ratio selection is essentially a system-level trade-off:

  • Higher reduction ratios bring stronger torque and higher control precision, but reduce motion speed and dynamic performance
  • Lower reduction ratios improve response speed and flexibility, but impose higher requirements on load capacity and control stability

Therefore, in robot joint design and actuator selection, reduction ratio cannot be optimized in isolation, but must be co-designed with motor torque density, reducer efficiency, and control system performance as an integrated whole.

With the development of humanoid robots and high-dynamic robot systems, future joint design is shifting from traditional "single reduction ratio optimization" toward system-level integrated actuator design (Actuator-Level Optimization)

 

Summary

In robot joint system design, reduction ratio is a core parameter running through overall performance. It not only determines the speed and torque conversion relationship from motor output to the joint end, but also profoundly affects the joint's dynamic response capability, control precision, and system stability. Therefore, in the robot design process, reduction ratio selection is often directly related to the upper limit of overall system performance.

From the mechanism of action, reduction ratio is essentially an energy redistribution between "speed" and "torque". Higher reduction ratios can significantly improve output torque and control precision, but reduce motion speed and dynamic response capability; while lower reduction ratios can bring faster response speed and motion flexibility, but have certain limitations in load capacity and system stiffness.

In different application scenarios, the differences in reduction ratio selection are particularly evident. Humanoid robots typically need to strike a balance among strength, speed, and flexibility; quadruped robots place more emphasis on dynamic response and lightweight design, thus tending toward lower reduction ratios; while industrial manipulators focus more on high precision and high stiffness, typically adopting higher reduction ratios to ensure stable load capacity and positioning accuracy.

Therefore, there is no universally optimal solution for reduction ratio design; it is a typical system-level trade-off problem. It requires overall optimization combining motor performance, reducer efficiency, load requirements, and control system capabilities.

As robotics technology advances toward high dynamics, high precision, and high integration, reduction ratio optimization is evolving from a single parameter selection into one of the core elements of collaborative design for overall joint systems.

Back to blog