Before Purchasing a Gimbal Motor, Which Key Parameters Must Be Compared?

Before Purchasing a Gimbal Motor, Which Key Parameters Must Be Compared?

With the rapid development of drones, robots, electro-optical pods, and intelligent vision devices today, the stability and control accuracy of gimbal systems are becoming increasingly important. However, many projects face the same question in the early stages of development: Why do gimbal motors with seemingly similar parameters perform so differently?

Some motors enable smooth and stable target tracking, while others suffer from jitter, slow response, or even severe heating. The reason often lies not in the control algorithm, but in neglecting the comparison and evaluation of key parameters during the procurement phase.

In fact, the gimbal motor not only determines the motion performance of the device but also directly affects the system's stability, response speed, and long-term reliability. For applications demanding high-precision control, selecting the right gimbal motor is often a critical factor in project success.

 

What is a Gimbal Motor?

A Gimbal Motor is a type of motor specifically designed to control the attitude and motion of a gimbal, enabling precise rotational control of the Pitch, Roll, and Yaw axes. Compared to ordinary drive motors, gimbal motors place greater emphasis on low-speed stability, control precision, and fast response capability, ensuring the device remains stable during motion or when subjected to external disturbances.

Gimbal motors are widely used in drone gimbals, robotic vision systems, electro-optical pods, security surveillance equipment, and surveying instruments, serving as the core component for ensuring system stability, tracking accuracy, and dynamic response capability. Therefore, when procuring gimbal motors, it is crucial to understand their key performance parameters and make reasonable selections to enhance overall device performance.

 

Why is Gimbal Motor Selection So Important?

The gimbal motor is the core component enabling precise motion control and stable attitude maintenance in a gimbal system, and its performance directly affects device operation. Whether for drone aerial photography, robotic vision systems, or electro-optical pods and surveying equipment, the gimbal relies on the motor to continuously counteract external vibrations and motion disturbances, ensuring the target remains stable.

If the motor is improperly selected, even advanced control algorithms may result in decreased tracking accuracy, sluggish response, image jitter, severe heating, and other issues. At the same time, improper selection can increase system power consumption, shorten device lifespan, and raise maintenance costs.

Therefore, when procuring gimbal motors, beyond size and price, it is essential to focus on evaluating key parameters such as torque, encoder accuracy, moment of inertia, cogging torque, and communication interface. Only by selecting a motor that matches the application requirements can the performance advantages of the gimbal system be fully realized, ensuring long-term stable operation.

 

Which Key Parameters Must Be Compared for Gimbal Motors?

Performance differences in gimbal motors often lie in detailed parameters. For applications requiring high stability and high-precision control, focusing solely on motor power or size is far from sufficient. To ensure smooth operation, precise tracking, and long-term reliability of the gimbal system, the following key parameters should be compared before procurement.

1. Torque

Torque is the core indicator of a gimbal motor's output capability.

Key points to focus on:

  • Rated Torque: The stable output capability of the motor during long-term continuous operation
  • Peak Torque: The maximum torque the motor can output for a short period

Insufficient torque may prevent the motor from stably driving the load, leading to reduced tracking accuracy or sluggish response. Therefore, a certain torque margin should be预留 based on load weight and motion requirements.

2. Encoder Accuracy

The encoder determines the motor's position feedback accuracy.

Higher encoder resolution results in:

  • More precise positioning
  • Smoother motion
  • Smaller tracking errors

For visual tracking, surveying equipment, and high-precision robotic applications, a high-resolution encoder is often a critical condition for ensuring control effectiveness.

3. KV Value

The KV value reflects the motor's speed characteristics.

Generally speaking:

  • Low KV value motors provide higher output torque
  • They operate more smoothly
  • They are more suitable for high-precision gimbal control

For most gimbal applications, low KV designs typically achieve better control performance.

4. Cogging Torque

Cogging torque is a major cause of vibration when the motor operates at low speeds.

If cogging torque is significant, it may lead to:

  • Unstable low-speed operation
  • Image jitter
  • Decreased tracking accuracy

Therefore, high-performance gimbal motors often use optimized magnetic circuit designs to reduce the cogging effect.

5. Moment of Inertia

Moment of inertia affects the motor's dynamic response capability.

The smaller the inertia:

  • The faster the start/stop speed
  • The more responsive the control
  • The better the tracking performance

For gimbal systems requiring fast target tracking, a low-inertia design offers significant advantages.

6. Motor Size and Weight

In applications such as drones and mobile robots, motor size and weight directly impact overall system performance.

During procurement, attention should be paid to:

  • Outer diameter
  • Motor length
  • Installation space
  • Total weight

Choosing a more compact and lightweight solution, while meeting performance requirements, is generally more beneficial for system design.

7. Operating Voltage and Power

Different devices have different power supply platforms, so it is necessary to confirm whether motor parameters match the system's power supply.

Key comparison points:

  • Rated voltage
  • Rated current
  • Peak power
  • Driver compatibility

Proper electrical matching improves system efficiency and reduces the risk of failure.

8. Protection Rating

If the equipment needs to operate in complex environments, protection capability is equally important.

Common indicators to consider:

  • IP54: Basic dust and water resistance
  • IP65: Strong dust and water resistance
  • IP67: Suitable for harsh environments

For outdoor equipment, vehicle-mounted platforms, and marine applications, a high protection rating effectively enhances reliability.

9. Operating Temperature Range

Different application environments have varying requirements for motor temperature adaptability.

Examples include:

  • Industrial environments
  • Outdoor equipment
  • Extremely cold regions
  • High-temperature environments

A wide temperature range design ensures stable motor operation under complex conditions.

10. Communication Interface and Control Method

Modern gimbal systems increasingly rely on intelligent control, making the communication interface an important selection criterion.

Common interfaces include:

  • CAN Bus
  • CAN FD
  • RS485
  • UART
  • EtherCAT
  • Modbus

Standardized communication protocols reduce development difficulty and improve system integration efficiency.

11. Motor Structure Type

Different gimbal motor structures are suitable for different scenarios.

Common types include:

  • Outer rotor brushless motors: Lower cost, widely used
  • Frameless torque motors: High torque density, high-precision control

In high-end gimbal systems, frameless torque motors are increasingly becoming the mainstream choice.

 

Gimbal Motor Selection Recommendations

Facing different application scenarios, no single gimbal motor can meet all requirements. Therefore, during the selection process, a comprehensive evaluation should be conducted based on factors such as load weight, control accuracy, installation space, and operating environment.

Select Torque Based on Load Requirements

Torque is the primary basis for selection. It is recommended to calculate the required torque based on the gimbal load weight and motion requirements, and reserve a certain safety margin to ensure stable operation during acceleration, deceleration, or external disturbances.

For light-load gimbal systems, consider the CubeMars GL40 series; for industrial gimbals and electro-optical pods requiring higher output capability, the CubeMars GL60 and CubeMars GL80 series can provide higher continuous torque output.

Select Encoder Based on Control Accuracy

For applications involving visual tracking, surveying equipment, or high-precision positioning systems, priority should be given to gimbal motors equipped with high-resolution encoders to achieve more precise position feedback and smoother motion control.

For example, the CubeMars GL40 II KV 82.5 and GL60 II KV 28 series support high-precision position feedback, meeting the positioning accuracy requirements of robotic vision systems, surveying equipment, and intelligent monitoring platforms.

Select Moment of Inertia Based on Dynamic Performance

For applications requiring fast response and high-speed tracking, it is advisable to choose motors with lower moment of inertia. Lower inertia improves system response speed and enhances dynamic control performance.

In drone gimbals and high-speed target tracking scenarios, the CubeMars GL40 II KV 82.5, with its low rotor inertia and fast response characteristics, achieves more sensitive and smoother motion control.

Select Motor Structure Based on Installation Space

When internal device space is limited, focus on motor size, weight, and integration method.

For space-constrained compact gimbal designs, the CubeMars GL40 II KV 82.5 offers high power density and a compact structure; for systems requiring greater load capacity, the CubeMars GL60 II KV 28 or GL80 series can be selected to maintain torque output while optimizing overall structural layout.

Select Protection Rating Based on Operating Environment

For outdoor, vehicle-mounted, marine, or industrial environments, focus on the motor's dust protection, water resistance, and ability to withstand high and low temperatures.

Some CubeMars gimbal motor products feature optimized structural designs and reliable material solutions, adapting to complex industrial environments and long-term continuous operation. During actual selection, confirm the protection rating and environmental adaptability of the corresponding products based on specific project requirements.

Select Communication Interface Based on System Architecture

In robotics and automation equipment, the communication interface directly affects system integration efficiency. It is recommended to prioritize products supporting mainstream protocols such as CAN Bus, CAN FD, EtherCAT, or RS485 for quick compatibility with existing control systems.

 

Conclusion

With the rapid development of the drone, robotics, and intelligent equipment industries, the requirements for motion control precision and stability in gimbal systems are continuously increasing. As the core actuating component of the gimbal system, the quality of gimbal motor selection directly determines device performance.

During the procurement process, it is recommended to focus on key parameters such as torque, encoder accuracy, KV value, cogging torque, moment of inertia, motor structure, protection rating, and communication interface, rather than simply comparing price or power. Only by selecting products that highly match actual application requirements can the performance advantages of the gimbal system be fully realized, achieving more precise, stable, and reliable motion control.


Back to blog