Design Trade-offs of High-Torque Outer Rotor Motors in Robotics: How to Balance Torque, Efficiency, and Reliability?

Design Trade-offs of High-Torque Outer Rotor Motors in Robotics: How to Balance Torque, Efficiency, and Reliability?

With the development of humanoid robots, quadruped robots, collaborative robots, and industrial robotic arms, robot joints are demanding higher performance from their actuation systems. Traditional motor solutions are gradually struggling to meet the robotics industry's requirements for high torque density, high response speed, compact structure, and precise control.

High-torque outer rotor motors, leveraging their unique structural advantages, have become an important technological approach in robotic joint actuation systems. However, in actual design practice, outer rotor motors are not simply about pursuing greater torque; rather, they require a comprehensive trade-off among torque output, weight, efficiency, heat dissipation, inertia, and reliability.

This article will provide an in-depth analysis of the key design factors for high-torque outer rotor motors in robotic applications, as well as the technical challenges that need to be considered during engineering development.

 

What is a High-Torque Outer Rotor Motor?

 

An outer rotor motor is a motor structure where the rotor is located on the outside of the stator. Unlike traditional inner rotor motors, the outer rotor design increases the rotor diameter, thereby enlarging the effective radius for magnetic field interaction and increasing the output torque per unit volume.

Its basic structure includes:

1.External Rotating Rotor

  • Integrates permanent magnets
  • Provides a larger effective torque radius

2.Internal Fixed Stator

  • Contains winding structures
  • Responsible for generating the rotating magnetic field

3.Bearings and Support Structure

  • Ensures stability during high-speed rotation

Since torque is:

T = F × r

where a larger r (radius arm) leads to higher theoretical output torque, the outer rotor structure is naturally suited for robotic applications requiring high torque output.

 

Why Do Robots Need High-Torque Outer Rotor Motors?

 

The key difference between robotic joints and ordinary industrial motors lies in the fact that:

Robots not only need to move, but also require:

  • Fast response
  • Precise control
  • High peak torque
  • High-frequency dynamic changes
  • Long-term stable operation

For example, the leg joints of a humanoid robot need to instantly output high torque during actions such as:

  • Standing up
  • Walking
  • Jumping
  • Maintaining balance

Traditional motors typically require a gearbox to increase torque, but the reduction system introduces:

  • Friction losses
  • Backlash errors
  • Response delays
  • Increased mechanical complexity

Therefore, high-torque-density outer rotor motors represent an important solution for reducing reliance on mechanical transmission.

 

Core Advantages of Outer Rotor Motor Design

 

I. Higher Torque Density

The greatest advantage of the outer rotor structure is its larger effective magnetic field radius.

Compared to inner rotor motors, under the same volume conditions:

  • Higher torque output
  • Stronger peak torque capability
  • Higher power density

This is critical for robotic joints because the internal space in robots is limited, and it is necessary to maximize the output capability per unit weight.

Typical applications include:

  • Humanoid robot knee joints
  • Quadruped robot hip joints
  • Pan-tilt rotation mechanisms
  • Robotic arm joints

II. More Compact Integrated Design

Robotic joints typically require a high level of integration of:

  • Motor
  • Encoder
  • Driver
  • Reduction mechanism

Due to their potential for a large hollow space design, outer rotor motors can conveniently integrate:

  • Cables
  • Bearings
  • Encoders
  • Sensors

to form a more compact joint module.

This is why many robot manufacturers adopt an integrated actuator solution combining:

Motor + Gearbox + Driver + Controller

III. Better Low-Speed Performance

Robotic movements usually do not involve high-speed rotation but rather:

  • Low speed
  • High load
  • High-precision control

Due to their strong torque output capability, outer rotor motors maintain excellent:

  • Torque stability
  • Control response
  • Motion smoothness

at low speeds.

They are particularly well-suited for:

  • Collaborative robots
  • Dexterous hands
  • Exoskeleton robots

 

Key Design Trade-offs for High-Torque Outer Rotor Motors

 

1. Torque vs. Rotational Inertia

Increasing torque typically involves:

  • Enlarging rotor dimensions
  • Adding magnet weight
  • Increasing the effective radius

However, the outer rotor structure inherently increases rotational inertia.

An increase in rotational inertia can lead to:

Advantages:

  • More stable motion
  • Enhanced load resistance

Disadvantages:

  • Reduced acceleration
  • Slower response speed
  • Increased control difficulty

For robotics, higher torque is not always better.

The design goal must balance:

High torque output + Fast dynamic response

For example:

  • Legged robots prioritize peak torque
  • Robotic arms prioritize response speed
  • Dexterous hands prioritize low inertia

II. Torque Density vs. Heat Dissipation Capability

Higher torque demands higher current, and increased current generates more heat.

Motor losses primarily include:

Copper losses:


P = I²R — the higher the current, the more pronounced the winding heating.

 

Iron losses:

  • Hysteresis losses
  • Eddy current losses

In robotic applications, inadequate heat dissipation design can lead to:

  • Torque reduction
  • Decreased efficiency
  • Shortened motor lifespan

Therefore, high-performance outer rotor motors typically require:

  • Optimized winding design
  • Higher slot fill factor
  • Improved heat conduction paths
  • Use of potting technology

For example, potted motors can enhance:

  • Dust and moisture resistance
  • Vibration reliability
  • Heat transfer efficiency

making them suitable for long-term robot operation environments.

III. High Power Density vs. Reliability

To improve performance, engineers typically:

  • Increase magnetic flux density
  • Increase current density
  • Reduce structural dimensions

However, these measures all increase design stress.

Considerations include:

Magnet Reliability
During high-speed operation:

  • Centrifugal force increases
  • Magnet fixation requirements become more stringent

Bearing Life
Robotic joints undergo frequent:

  • Forward and reverse rotation
  • Impact loads
  • Dynamic motion

which impose higher demands on bearing life.

Structural Stiffness
Robotic joints need to withstand:

  • External impacts
  • Heavy-load holding
  • High-frequency motion

Therefore, the mechanical structure must balance lightweight design with rigidity.

 

Matching Outer Rotor Motors with Robot Gearboxes



Solution Characteristics Advantages Limitations
Outer rotor motor direct drive Motor directly outputs Fast response, zero backlash Limited torque
Outer rotor motor + planetary gearbox High rigidity High load capacity, high efficiency Complex structure
Outer rotor motor + harmonic gearbox High reduction ratio High precision Lower rigidity

 

In practice, the choice depends on the robot's requirements.

For example:

Humanoid Robots
Focus on:

  • High peak torque
  • High dynamic response
  • Lightweight design

Typically adopt:
High-torque motor + high-performance gearbox.

Industrial Robotic Arms
Focus on:

  • Precision
  • Rigidity
  • Long-term operation

Require:
High-reliability motor + high-rigidity transmission solution.

Quadruped Robots
Focus on:

  • Explosive power
  • Impact resistance
  • Rapid movement

Emphasize:
Peak torque and mechanical strength.

 

Future Development Trends of High-Torque Outer Rotor Motors

 

With the advancement of robotics technology, outer rotor motors will evolve towards the following optimizations:

1.Higher Torque Density
Through:

  • High-performance magnetic materials
  • Electromagnetic design optimization
  • Higher slot fill factor windings
    to enhance output per unit weight.

2.Greater Intelligence
Future robotic joints will integrate:

  • Encoders
  • Torque sensors
  • Temperature sensing
  • Intelligent control algorithms
    to achieve more precise motion control.

3.Higher Reliability
For long-term robotic operation requirements:

  • Potting technology
  • High-performance bearings
  • Optimized heat dissipation structures
    will become key technological directions.

 

How to Choose a Suitable High-Torque Outer Rotor Motor for Robotics?

 

When selecting a motor, it is necessary to comprehensively consider:

① Torque Requirements
Focus on:

  • Continuous torque
  • Peak torque
  • Load variations

② Speed Requirements
Different robotic applications:

  • Pan-tilts require fast response
  • Robotic arms require precise control
  • Humanoid robots require dynamic movement

③ Weight and Size Constraints
Robot space is limited, requiring:

  • High power density
  • Compact design

④ Thermal Management Capability
Verify:

  • Continuous operation time
  • Cooling method
  • Operating environment

⑤ Control Compatibility
Modern robot motors need to support:

  • High-resolution encoders
  • CAN communication
  • EtherCAT
  • Real-time control

 

Conclusion

 

High-torque outer rotor motors, with their unique structural advantages, are becoming a key technological solution in robotic actuation systems. Compared to traditional inner rotor motors, the outer rotor design enhances the output torque and torque density per unit volume by increasing the effective magnetic field radius, providing stronger power output within a limited installation space. This feature makes them highly suitable for application scenarios such as humanoid robots, quadruped robots, collaborative robots, and industrial robotic arms that demand high-performance joint actuation.

However, in robotic applications, high torque is not the sole design objective. In actual development, a comprehensive trade-off must be made among torque, rotational inertia, response speed, heat dissipation capability, and long-term reliability. Overemphasizing torque may increase rotor weight and inertia, thereby reducing the robot's motion agility; simultaneously, boosting power density introduces greater thermal management challenges. Therefore, an optimal robotic motor design must achieve a balance between dynamic performance and system reliability through optimized electromagnetic structures, enhanced heat dissipation efficiency, and reinforced mechanical strength.

As the robotics industry rapidly advances towards lightweight construction, high dynamics, high precision, and intelligence, high-torque outer rotor motors are undergoing continuous optimization and upgrades. By integrating high-performance magnetic materials, advanced manufacturing processes, potting technology, and intelligent control systems, future robot motors will achieve higher efficiency, greater environmental adaptability, and extended service life, providing core power support for robots to perform more precise, natural, and high-load movements.

For robotics developers, selecting the appropriate high-torque outer rotor motor requires a comprehensive evaluation based on specific application needs, including output torque, speed range, structural dimensions, cooling conditions, control methods, and operating environment. Only by finding the optimal balance between power performance and system requirements can the advantages of outer rotor motors be fully leveraged, driving robotic joints towards higher performance, greater reliability, and enhanced intelligence.

Back to blog